T_DemodFreqUnit
This is a Data Header variable.
Type = Short
The value of T_DemodFreqUnit indicates whether the x- or z-axis units (if applicable) were hertz (0) or carrier (1) when the trace was saved. This only applies if either the x- or z-axis units are frequency units.
The T_ variables describe the display setup when the trace was saved. When you recall and display a saved trace, the VSA uses the T_ variables to restore the display settings to their settings when the trace was saved.