T_DemodSymbolShape
This is a Data Header variable.
Type = Short
The value of T_DemodSymbolShape indicates the Symbol Shape when the trace was saved.
- 0 = None
- 1 = Dots
- 2 = Bars
The T_ variables describe the display setup when the trace was saved. When you recall and display a saved trace, the VSA uses the T_ variables to restore the display settings to their settings when the trace was saved.