T_YRefTrackRange
This is a Data Header variable.
Type = Boolean
When T_YRefTrackRange is true, the Y Reference Level will track the input channel range.
The T_ variables describe the display setup when the trace was saved. When you recall and display a saved trace, the VSA uses the T_ variables to restore the display settings to their settings when the trace was saved.