Text (Multitone Definition Files)
Sharing Data With Other Applications
Some optional measurement types (e.g., Component Test Measurement) support saving and recalling multitone definition files from within the measurement's parameter dialog. The file format is also compatible with N7621 Signal Studio for Multitone Distortion exported multitone definitions.
The text (*.TXT) format looks like the following example:
Enabled RelativeFrequencyInHz GainInDB PhaseInDegrees
1 -1820000000 0 0
1 -1300000000 0 0
1 -780000000 0 0
1 -260000000 0 0
1 260000000 0 0
1 780000000 0 0
1 1300000000 0 0
1 1820000000 0 0
Enabled: 0-Enabled; 1-Disabled
RelativeFrequencyInHz: All tones must have constant tone spacing to be compatible with component test measurement. 0 Hz is equivalent to the measurement center frequency.
See Also