TrcLedBold
This is a Data Header variable.
Type = Boolean
When TrcLedBold is available it is set by the measurements when a trace LED is set. TrcLedBold is available for "NO DATA" and "OV" only.
This is a Data Header variable.
Type = Boolean
When TrcLedBold is available it is set by the measurements when a trace LED is set. TrcLedBold is available for "NO DATA" and "OV" only.
|
Copyright © 2000-2026 Keysight Technologies, Inc. |