TrcLedStr
This is a Data Header variable.
Type = String
When TrcLedStr is available, it contains the trace LED string. The LED string is displayed in the Trace indicator. For a list of possible strings, see Trace indicators .
This is a Data Header variable.
Type = String
When TrcLedStr is available, it contains the trace LED string. The LED string is displayed in the Trace indicator. For a list of possible strings, see Trace indicators .
|
Copyright © 2000-2026 Keysight Technologies, Inc. |