TS_SumDataWidth
This is a Data Header variable.
Type = Int
TS Technical Specification_SumDataWidth is the number of counts in a horizontal scan line for a trace with Cumulative History enabled.
See Also
This is a Data Header variable.
Type = Int
TS Technical Specification_SumDataWidth is the number of counts in a horizontal scan line for a trace with Cumulative History enabled.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |