TstLimCount
This is a Data Header variable.
Type = Short
TstLimCount indicates the number of limit tests for current trace. There can be up to 4 composite limit result lines: an upper limit line, an upper margin line, a lower limit line, and a lower margin line.