TstLim*Display
This is a Data Header variable.
Type = Short
In Limit Tests, TstLim*Display indicates which lines to display (limit, margin, or both) in the composite limit test.
The values for TstLim*Display are:
- 1 = Limit
- 2 = Margin
- 3 = Both
The '*' in TstLim*Display indicates the limit test number, the first limit test being 1 (i.e. TstLim1Display, TstLim2Display and so on).