TstLim*Draw
This is a Data Header variable.
Type = Short
In Limit Tests, TstLim*Draw indicates how to draw between the points (one line or connected points) in the composite limit test.
The values for TstLim*Draw are:
- 0 = One Line
- 1 = Connected Points
The '*' in TstLim*Draw indicates the limit test number, the first limit test being 1 (i.e. TstLim1Draw, TstLim2Draw and so on).