TstLim*Fail
This is a Data Header variable.
Type = Short
In Limit Tests, TstLim*Fail indicates how to show the trace if the limit fails (in trace color or in fail color) in the composite limit test.
The values for TstLim*Fail are:
- 0 = In Trace Color
- 1 = In Fail Color
The '*' in TstLim*Fail indicates the limit test number, the first limit test being 1 (i.e. TstLim1Fail, TstLim2Fail and so on).