TstLim*Reason
This is a Data Header variable.
Type = String
In Limit Tests, if TstLim*Result is None, TstLim*Reason is the reason the limits were not tested.
The '*' in TstLim*Reason indicates the limit test number, the first limit test being 1 (i.e. TstLim1Reason, TstLim2Reason and so on).