TstLim*Result
This is a Data Header variable.
Type = Short
In Limit Tests, TstLim*Result indicates the result (none, pass or fail) of the limit test.
The values for TstLim*Result are:
- 0 = None
- 1 = Pass
- 2 = Fail
The '*' in TstLim*Result indicates the limit test number, the first limit test being 1 (i.e. TstLim1Result, TstLim2Result and so on).