TstLim*YSide
This is a Data Header variable.
Type = Short
In Limit Tests, TstLim*YSide indicates the side (upper or lower) of the limit test. There can be two composite limit tests, one for upper limits and one for lower limits.
The values for TstLim*YSide are:
- 0 = Upper
- 1 = Lower
The '*' in TstLim*YSide indicates the limit test number, the first limit test being 1 (i.e. TstLim1YSide, TstLim2YSide and so on).