XSegmentDomain
This is a Data Header variable.
Type = Short
XSegmentDomain indicates the domain of the z axis. The domain depends upon the type of data displayed in the trace. OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Error Vector Spectrum has an XSegmentDomain = 2 (Time) and Error Vector Time has an XSegmentDomain = 1 (Frequency).
- 0 = Unknown
- 1 = Frequency
- 2 = Time
- 3 = Channel
- 4 = Amplitude