XSegmentLen
This is a Data Header variable.
Type = Long
When OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. data has a z-axis (e.g. Error Vector Spectrum), XSegmentLen is the number of consecutive number of x-y pairs associated with each z-axis value. For example, with Error Vector Spectrum, XSegmentLen is the number of carriers in each symbol.