Yn_m
This is a Data Header variable.
Type = Array of numbers
Yn_m is the header for the list of Y-axis values for channel n of a m-channel measurement. If this is complex data, the data is in real/imaginary pairs.
For example Y3_8 would be the header for measurement channel 3's data in an 8 channel measurement.