YUnit
This is a Data Header variable.
Type = String
YUnit is a string indicating the Y axis units, for example, "V" or "dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer". The Y axis units depend on the kind of data displayed.
See Also