ZeroPadding
This is a Data Header variable.
Type = Double
ZeroPadding is a ratio (0.0 to 1.0) indicating how much zero padding to add to the time data before converting to frequency domain: 0 = no padding, 1.0 is all padding
For time data only, this is the zero-padding ratio for a subsequent FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum.. For frequency data this number is used to determine the time length for an FFT.
See Also