Pk CDE (TD-SCDMA)
Pk CDE (Composite Peak CDE) is the largest measured code channel Code Domain Error. This is the largest measured CDE for all code channels (active and inactive) in the base code layer (the code layer with the smallest symbol rate) in the composite signal.
See Also