Analysis CDF (TD-SCDMA)
trace data displays the cumulative distribution function (CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X.) for the and . CDF is computed by integrating the PDF 1) Probability Density Function Trace Data, or 2) Portable Document Format (PDF) created by Adobe Systems is an open standard for document exchange. (Probability Density Function).
For more information see CCDF (TD-SCDMA) and CDF.
and parameter entry shortcut: Right click on the desired Timeslot in the Overall Time trace data display, then select .
See Also