Analysis Spec (TD-SCDMA)
trace data is the spectral display of the pre demodulated Time data for the selected Sub-frame (SF 1) Spreading Factor, or 2) service flow: A unidirectional flow of medium access control (MAC) service data units (SDUs) on a connection that is provided a particular Quailty of Service (QoS).) and Timeslot (TS Technical Specification). The Time data is Windowed and FFTed to create the Spectrum display.
If averaging is on, trace data is the averaged trace data. When averaging is set to zero, the trace data is equal to the trace data.
and parameter entry shortcut: Right click on the desired Timeslot in the Overall Time trace data display, then select .
See Also