Inst Analysis Spec (TD-SCDMA)
trace data is the spectral display of the pre demodulated Time data for the selected (SF 1) Spreading Factor, or 2) service flow: A unidirectional flow of medium access control (MAC) service data units (SDUs) on a connection that is provided a particular Quailty of Service (QoS).) and (TS Technical Specification). It uses the non-averaged time data and is not affected by averaging.
Averaging
Averaging does not affect the trace data. Use the trace data to apply averaging to the spectral display. When averaging is set to OFF, the trace data is equal to the trace data.
and parameter entry shortcut: Right click on the desired Timeslot in the Overall Time trace data display, then select .
See Also