Composite Error Summary (TEDS)
The composite TEDS subcarriers). All measurements, except , , , and , depend on the symbols in the calculation. You can choose which symbols to include in the calculation using the Include Sync/Pilot Symbols and Include Header Symbols settings plus the effects of droop using Include Droop and also Pilot Tracking.
trace shows quality metrics for the composite TEDS signal (all validThe trace below is for a Normal Uplink, 50kHz channel bandwidth, 16QAM signal.
The
trace provides the following information:
Parameter |
Description |
---|---|
A summary of the composite EVM in %rms where the Root Mean Square (rms) of the error vectors is computed and expressed as a percentage of the square root of the mean power of the ideal signal. |
|
EVM Max |
Subcarrier with the maximum EVM in %rms and the TEDS subcarrier location. |
EVM Pk |
Symbol with the peak EVM in % and the symbol location on the specific TEDS subcarrier. |
Mag Err |
Composite symbol magnitude error in %rms. Magnitude error is the difference in amplitude between the I/Q measured signal and the I/Q reference signal and is an indicator of the quality of the modulated signal amplitude component. A high magnitude error might indicate, for example, incidental AM Amplitude Modulation - CW modulation using amplitude variation in proportion to the amplitude of the modulating signal. Usually taken as DSB-LC for commercial broadcast transmissions and DSB-SC for multiplexed systems. modulation on the signal. |
Mag Err Max |
Maximum symbol magnitude error in % and the specific TEDS subcarrier location. |
Mag Err Pk |
Peak symbol magnitude error in % and the symbol on the specific TEDS subcarrier location. |
Phase Err |
Composite IQ phase error in degrees. Phase error is the difference in phase between the I/Q measured signal and the I/Q reference signal and is an indicator of the quality of the modulated signal phase component. A high phase error might indicate, for example, incidental FM Frequency Modulation modulation on the signal. |
Phase Err Max |
Maximum IQ phase error in degrees and the specific TEDS subcarrier location. |
Phase Err Pk |
Peak IQ phase error in degrees and the symbol on the specific TEDS subcarrier location. |
Freq Err |
Composite frequency error in Hertz (or fractions of Hertz). This value is not subject to the symbols in the EVM calculation or Droop or Pilot Tracking. |
Freq Err Max |
Maximum frequency error in Hertz (or fractions of Hertz), and the specific TEDS subcarrier. This value is not subject to the symbols in the EVM calculation or Droop or Pilot Tracking. |
Freq Err Pk |
Peak frequency error in Hertz (or fractions of Hertz), and the symbol on the specific TEDS subcarrier location. This value is not subject to the symbols in the EVM calculation or Droop or Pilot Tracking. |
IQ Offset |
Composite subcarrier IQ offsets. is the average of allFor a single-carrier signal, IQ offset would indicate the magnitude of the carrier feedthrough, which is caused by offsets in the modulation inputs to the quadrature modulator. However, since composite subcarrier IQ offsets (and the center of an individual subcarrier is not aligned with the carrier center (0 Hz) of the combined signal), composite does not represent the magnitude of the carrier feedthrough. is based on theThis value is not subject to the symbols in the EVM calculation or Droop or Pilot Tracking. |
IQ Offset Max |
Maximum IQ Offset (also called I/Q origin offset) for a particular specific TEDS subcarrier. This value is not subject to the symbols in the EVM calculation or Droop or Pilot Tracking. |
Ref Pwr |
Average power of all sync and pilot symbols. |
Droop Rate |
Droop Rate refers to a transmission signal impairment that measures the amplitude difference between the start and end of a TDMA burst time division multiple access burst: A contiguous portion of the uplink or downlink using PHY parameters, determined by the Downlink Interval Usage Code (DIUC) or Uplink Interval Usage Code (UIUC), that remain constant for the duration of the burst. TDMA bursts are separated by preambles and are separated by gaps in transmission if subsequent bursts are from different transmitters.. It is calibrated in dB/symbol, typically in fractions, that is mdB/symbol (millidB) or udB/symbol (microdB). To remove droop correction from your measurements, clear the Include Droop checkbox. The droop rate is displayed regardless of whether Include Droop is selected. |
See Also