Correction (TEDS)
shows values that are applied to the acquired data to compensate for phase and magnitude anomalies in the measurement hardware and software signal processing, determined during calibration sequences. If a straight line, then there is no correction.
Select to scale the trace. If the trace shows NO DATA, check your recorded signal or hardware input and TEDS demod properties.
See Also