Main Time (TEDS)

Main Time trace shows a block of time-record samples of the signal waveform from which time, frequency, and modulation domain data is derived. This time record length (main time) represents a slot length. For Normal Downlink and Normal Uplink, the time scale is a nominal 14.167msec, while the Random Access and Control Uplink time scale is a nominal 7.083msec.

Select Trace > Auto Scale to scale the trace.

For the Normal Downlink slot format, the main time trace is continuous while the Normal Uplink, Random Access Uplink, and Control Uplink slot formats show the propagation delay segments.

To learn more about setting the Main Time parameters, see Analysis > Time. To change the time scale, see Trace > Properties > X Scale.

See Also

About TEDS Trace Data