PvT Time (TEDS)
shows a non-complex time display with time = 0 aligned to the first symbol. The trace below is a Normal Uplink, 50kHz channel bandwidth, 16QAM modulation signal with a 14.167msec slot length. For the Normal Downlink slot format, the main time trace is continuous while the Normal Uplink, Random Access, and Control Uplink slot formats show the propagation delay segments.
The length of time before and after a burst can be specified using the PvT Off Analysis Time parameter in the Advanced Tab of the TEDS demodulation properties dialog. The and the are both set to 5msec (default) in the trace below
Select to scale the trace. Also choose the Y-axis units for the best display ( drop-down menu), however since the imaginary part is zero, many formats will be of no use.
See Also