Comp Error Vector Spec (W-CDMA(3GPP)/HSPA)
When W-CDMA Code Division Multiple Access: One of several digital wireless transmission methods in which signals are encoded using a specific pseudo-random sequence, or code, to define a communication channel. A receiver, knowing the code, can use it to decode the received signal in the presence of other signals in the channel. This is one of several "spread spectrum" techniques, which allows multiple users to share the same radio frequency spectrum by assigning each active user an unique code. CDMA offers improved spectral efficiency over analog transmission in that it allows for greater frequency reuse. Other characteristics of CDMA systems reduce dropped calls, increase battery life and offer more secure transmission. See also IS-95.(3GPP) Demodulation is enabled, the composite trace shows the frequency spectrum of the composite Error Vector Time trace data. In other words, the VSA derives the composite trace data and then windows and FFTs the data to produce the composite trace data.
The trace data is computed from the first slot in the after the (see Measurement Interval and Offset).
Marker Frequency Correction
The VSA's demodulator removes carrier-frequency error. Therefore, in the composite display the carrier-frequency error must be added to marker readouts to obtain exact frequency information. The carrier-frequency error () is shown in the composite Error Summary Table.
See Also