Composite IQ Offset (W-CDMA(3GPP)/HSPA)
(also called I/Q origin offset) indicates the magnitude of the carrier feedthrough signal. When there is no carrier feedthrough, IQ offset is zero (-infinity dB).
This parameter is the same as the digital demod IQ Offset except that the source data is the composite signal. See Digital Demod IQ Offset for further information about this parameter.
See Also