Composite Magnitude Error (W-CDMA(3GPP)/HSPA)
Composite Magnitude Error () is the difference in amplitude between the I/Q measured signal and the I/Q reference signal for the composite signal.
The display shows these Magnitude error values; the RMS (root mean square) Magnitude Error, the Peak (largest) Magnitude Error, and the chip number with the Peak Magnitude Error.
This error data is the same as the channel Magnitude Error except that the source data is the composite signal. See Despread Channel Magnitude Error for further information about this parameter.
See Also