Maximum Result Length (802.11b/g DSSS/CCK/PBCC)
The value is shown in the text box to the right of .
specifies the maximum number of chips that can be included in the measurement result length when is selected. The number of chips is rounded to the nearest whole number of data symbols, as determined from the input signals data rate and modulation format.
See Also