CCDF Summary (802.11b/g DSSS/CCK/PBCC)
The following table lists the CCDF Complementary Cumulative Distribution Function Summary data.
-
Average Power - Average input power (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer)
-
% at Power Average - % at Power Average is the probability that a random sample will be above the average power.
-
Relative Peak Power - Peak power (dB), relative to the average power level in dBm. This value shows how many dB the peak is above the average.
-
Absolute Peak Power - Absolute peak power (dBm)
-
Power at n% - The x-axis value (power in dB) of the CCDF curve at which the y-axis value is n%. Based on the data used to create the CCDF, the probability is n% that a point will have a power level that is above the "Power at n%" value. These values are computed using linear interpolation between CCDF bins. If there's not enough data in the CCDF to compute a value, *** will be displayed.
-
Points - Number of points accumulated
See Also