Spectral Emission Mask (802.11n/ac/ax/be/bn)

Spectral Emission Mask shows the Spectrum of the detected WLAN WLAN - Wireless Local Area Network: A system that includes the distribution system (DS), access points (APs), and portal entities. It is also the logical location of distribution and integration service functions of an extended service set (ESS). A WLAN system contains one or more APs and zero or more portals in addition to the DS. burst, with SEM limit lines overlaid. It is a frequency-domain display (power vs. frequency) that allows the user to visually see out-of-band emissions relative to the spectral mask defined by the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.11 standard.

The following limit lines are displayed on this trace:

How Limit Lines Are Determined

Limit lines are generated automatically based on the detected packet standard and channel bandwidth of the demodulated WLAN burst, per the IEEE 802.11 specifications.

Standard Supported Bandwidths
802.11n 20 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second., 40 MHz
802.11ac 20 MHz, 40 MHz, 80 MHz, 160 MHz
802.11ax 20 MHz, 40 MHz, 80 MHz, 160 MHz
802.11be 20 MHz, 40 MHz, 80 MHz, 160 MHz, 320 MHz
802.11bn 20 MHz, 40 MHz, 80 MHz, 160 MHz, 320 MHz

Measurement Parameters (RBW / VBW)

The SEM computation uses standard-specific resolution and video bandwidth targets:

Standard RBW Resolution Band Width (RBW or ResBW): specifies the minimum frequency bandwith that two separate frequency spectra can be resolved and viewed seperately. For FFT (digital) based VSA's the process is equivalent to passing a time-domain signal through a bank of bandpass filters, whose center frequencies correspond to the frequencies of the FFT bins. For a traditional swept-tuned (non-digital) spectrum analyzer, the resolution bandwidth is the bandwidth of the IF filter which determines the selectivity. RBW
802.11a / 11n / 11ac 100 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). 30 kHz
802.11ax / 11be / 11bn 100 kHz 7.5 kHz

Since the SEM is computed from the same acquisition used for demodulation (rather than a dedicated SEM acquisition), the actual achievable RBW/VBW depends on the burst length. If the burst is too short, the measurement still runs but a DATA? indicator warns the user that the RBW/VBW requirement was not met. The solution is to increase the number of data symbols in the transmitted PPDU PLCP Protocol data unit.

The RBW is the -3 dB bandwidth for the Gaussian Top window.

See Also

SEM Results

Available Trace Data (802.11n/ac/ax/be/bn)