CPE (802.11n/ac/ax/be/bn)
(Common Pilot Error) is the RMS level of the Common Pilot Error trace data minus 1, expressed as a percentage of an ideal signal. Ideally the trace data has a magnitude of one and phase of zero. represents the deviation of the trace from the ideal and shows how much the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. burst drifts over time.
See Also
About Error Summary Data (802.11n/ac/ax/be/bn)