PilotEVM (802.11n/ac/ax/be/bn)

PilotEVM (Pilot Error Vector Magnitude) is the RMS value of the Error Vector Magnitudes, expressed in dB, of the pilot subcarriers, averaged over all analyzed OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbols in the burst.

See Also

About Error Summary Data (802.11n/ac/ax/be/bn)

Available Error Summary Data (802.11n/ac/ax/be/bn)