EVMPeak (802.11n/ac/ax/be/bn)
is the peak level of the Error Vector Magnitude over all subcarriers and all analyzed OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbols. The value is shown in dB.
See Also