MIMO Channel Matrix (802.11n/ac/ax/be/bn)
is only available for multiple channel measurements.
shows the linear average over all subcarriers of the for each available channel/stream. Each value in the table is a complex value (displayed in real + j*imag format). The is used to look at the spatial spreading done by the transmitter.
This trace is not averaged even when averaging is enabled.
See Also
MIMO Ch Frequency Response (802.11n/ac/ax/be/bn)