PDF (802.11n/ac/ax/be/bn)
trace data displays the Probability Density Function of the selected channel. indicates the probability that a given level has occurred.
The is computed from the segment of the 802.11n/ac/ax/be/bn burst specified by the and . In addition, if the Offset is zero and the Interval is equal to the result length, the burst preamble is included in the .
See PDF for more detailed information about this trace data.
See Also