PDF (802.11a/g/j/p OFDM)
trace data displays the Probability Density Function of the selected channel. indicates the probability that a given level has occurred.
The is computed from the segment of the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. burst specified by the and . In addition, if the Offset is zero and the Interval is equal to the result length, the burst preamble is included in the .
See PDF for more detailed information about this trace data.
See Also