Raw Main Time (802.11a/g/j/p OFDM)
is the raw uncorrected time data acquired directly from input hardware or a playback recorded file. Raw Main Time is used to generate the Search Time data which is the resampled and corrected Raw Main Time data. The Search Length parameter is used to specify the amount of Raw Main Time data. The Search Length parameter is used to specify the amount of Raw Main Time data.
The Meas Setup " Time parameter is not available (disabled) when the VSA is in modulation analysis mode.
See Also
Search Time trace
Time trace