RMS Error Vector Time (802.11a/g/j/p OFDM)
The difference between and is the error vector, which would have a complex value at each subcarrier at each symbol. The looks at the error vector values for each symbol and does an RMS average of these values over all of the 52 used subcarriers. The result is a time trace, which shows the average error vector magnitude at each symbol.
See Also