Syms/Errs (802.11a/g/j/p OFDM)
When 802.11a/g/j/p OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demodulation is enabled, the trace data shows the symbol table trace data for OFDM demodulation. The symbol table shows you error summary data and the symbol data (raw binary bits) for each OFDM symbol and subcarrier following the preamble. See following topics for information about the symbol table and error summary data:
Available OFDM Error Summary Data
See Also