CDE Composite Trace Data (1xEVDO)
trace data shows the Code Domain Error (CDE) value for each active code channel () for all code layers (), along with the CDE value for each inactive code channel at the lowest code layer. The CDE of a particular code channel is a measure of the error power in a code channel relative to the total signal power.
Available only for reverse link direction channels.
trace data results are computed from the first measured half (0.5) slot. This is different than trace data results, which use Measurement Interval and Offset to determine the measurement data.
Display Format
The data is shown in a multi-color format that assigns a unique color to each code layer and related active code channels. This makes it easy to visually identify and distinguish the active code channels () for a given code layer (). The colors are also user definable (see Display Preferences > Color tab).
For and trace data displays with separate I/Q channel trace bars, to position the Marker to the desired Code Layer/Channel bar, click in close proximity to the horizontal bar that indicates the value of the code channel being measured.
Use the trace data to view only one code layer () at a time.
See Also