Inst CDP Composite (1xEVDO)
trace data shows the trace data for the Composite signal. It is the non-averaged CDP Composite trace data.
trace data results are computed from data specified by the Measurement Interval and Offset parameters. The forward link CDP composite results are for the specified (see Analysis Channel parameter). When is selected by , CDP measurements only exist for cases where the preamble length is detected to be 1024 chips.
trace data is not affected by averaging.
See Also