Error Summary (1xEVDO)
When 1xEV-DO Demodulation is enabled, selecting the Comp trace data shows the composite error summary data. This is the signal quality error summary information for the composite signal.
Composite, forward link, trace data results are computed from the first measured slot. Composite, reverse link, trace data results are computed from the first measured half (0.5) slot.
For more information see the following topics:
For the reverse link direction, there is also channel error summary trace data (), which provides the error information for a specific code channel and code layer (see About Channel Error Summary Data)
See Also