Spectrum (1xEVDO)
shows the spectral display of the pre-demodulated data. The data is windowed and FFTed to create the display (see VSA Concepts).
If averaging is on, trace data is the averaged trace data. When averaging is set to zero, the trace data is equal to the trace data.
VSA signal flow (see Digital Demodulation Block Diagram):
See Also