With a data trace active, click Tools, then Marker.
Then select a marker to place on the current trace. Place up to 6 markers on a trace.
Click Table to display or hide the marker table.
Click First 3 Peaks to add three markers to the highest peaks.
Drag a marker to move it.
Right-click on the marker to access marker-specific operations.
Markers can also be 'captured' with a trace.
Note: In NA mode Smith Chart format, markers can NOT be captured with traces, added, or moved . To include a marker on a Data Link trace in Smith Chart format, change the format to Log Mag, add a marker at the required frequency, then change format back to Smith Chart. To change format, right-click on the trace, then click Format.
Date Last Modified:
|
27-Sep-2011 |
Added smith Chart note |