|
(Read-Write) Causes the specified marker to become one of the SA Marker functions. Also causes the specified marker to be turned ON if it is not already. |
|
|
Relevant Modes |
SA |
|
Parameters |
|
|
<n> |
Existing marker to become a marker function. Choose from 1 to 6. |
|
<char> |
Marker function. Choose from: OFF - Marker is returned to it's previous state (normal or delta). NOISe - Marker becomes a noise marker. BPOWer - Marker becomes a Band/Interval Power marker. For non-zero span measurements, a Band Power marker integrates total power over the Band Power Span, which is set using: For Zero-span measurements, an Interval Power marker calculates the average power over the Interval Power Span, which is set using: |
|
Examples |
CALC:MARK1:FUNC NOIS |
|
Query Syntax |
CALCulate:MARKer<n>:FUNCtion? |
|
Default |
OFF |
Last Modified:
|
19-Oct-2010 |
New command (5.30) |