|
(Write-Read) Enables signal tracking utilizing the specified marker {1-6, default is 1}. If the specified marker is not already on, it is activated as a Normal marker. This marker then tracks the peak signal, via automatic changes to the Center Frequency. Any other markers that are active maintain their frequency position unless limited by Start or Stop Frequency. Note: Signal tracking is incompatible (inactive) with Zero Span.. |
|
|
Relevant Modes |
SA |
|
Parameters |
|
|
<bool> |
ON (1) - Enables signal tracking utilizing the specified marker, activating it if necessary. OFF (2) - Disables signal tracking. |
|
Examples |
CALC:MARK2:STR 1 'Marker 2 is set as the active signal tracking marker. |
|
Query Syntax |
CALC:MARK:STR? |
|
Default |
0 |
Last Modified:
|
26-sep-2016 |
Added new SA command (A.09.53) |