|
(Read-Write) Set and query measurement conversion function for the selected measurement. First select a measurement using CALCulate:PARameter:SELect. |
|
|
Relevant Modes |
NA |
|
Parameters |
|
|
<char> |
Conversion function. Choose from: OFF - No conversion ZAUTo - The displayed S-parameter is converted to the appropriate Z parameter: Refl for S11 and S22; Trans for S21 and S12. YAUTo - The displayed S-parameter is converted to the appropriate Y parameter: Refl for S11 and S22; Trans for S21 and S12. ZREFlection - The displayed S-parameter is converted to Z reflection, regardless of whether the S-parameter is reflection (S11 or S22) or transmission (S21 or S12). YREFlection - The displayed S-parameter is converted to Y reflection, regardless of whether the S-parameter is reflection (S11 or S22) or transmission (S21 or S12) ZTRansmissio - The displayed S-parameter is converted to Z transmission, regardless of whether the S-parameter is reflection (S11 or S22) or transmission (S21 or S12). YTRansmissio - The displayed S-parameter is converted to Y transmission, regardless of whether the S-parameter is reflection (S11 or S22) or transmission (S21 or S12). INVersion - The displayed S-parameter is converted to 1/S-parameter. |
|
Examples |
CALC:CONV:FUNC ZAUT |
|
Query Syntax |
CALCulate[:SELected]:CONVersion:FUNCtion? |
|
Return Type |
Character |
|
Default |
OFF |
Last Modified:
|
25-Mar-2014 |
New command (A.07.50) |